Addition
Adds 2 to 127 integer, real, TIME, or STRING variables.

Arguments | ||
|---|---|---|
(inputs) | SINT - USINT - BYTE - INT - UINT - WORD - DINT - UDINT - DWORD - LINT - ULINT - LWORD - REAL - LREAL - TIME - STRING | Can be of any integer, real, TIME, or STRING format. All inputs must have the same format. From 2 to 127 inputs. |
o1 | SINT - USINT - BYTE - INT - UINT - WORD - DINT - UDINT - DWORD - LINT - ULINT - LWORD - REAL - LREAL - TIME - STRING | Addition of the input terms. |
Example
(* FBD example with Addition Operators *)

(* ST equivalence: *)
ao10 := ai101 + ai102; ao5 := (ai51 + ai52) + ai53;
Provide Feedback