LD Rungs
Rungs are graphic components of Ladder Diagram (LD) programs and
represent a group of circuit elements leading to the activation of a coil. Rungs have labels
for identification within a diagram. Labels along with jumps enable controlling the
execution of a diagram. The label and jump must have the same name. When the connection on
the left of the jump element has the TRUE Boolean state, the diagram execution proceeds at
the label element. Comments are in rich text and inserted above the rung , for documentation
purposes only. To the left of a rung, a handle indicates the position within a diagram and
enables repositioning by dragging and dropping.
While dragging rungs from either the
toolbox or within a diagram, the language editor displays the possible drop points. Drop
points are displayed as plus signs in a black circle. For rungs, the possible drop points
are displayed between the rung handles on the left.
Drop points between rung handles
while dragging a rung in a diagram
Task | Procedure |
|---|---|
Insert a rung |
|
Drag a rung | When dragging rungs, the possible drop points are displayed between the handles
on the left.
|
Define the label for a rung |
|
Define the comment for a rung | Place comments in the space above the rung. After entering text, click elsewhere
in the workspace to 'validate' the comment.
|
Provide Feedback