Comment fields
All comment fields support plain text. Comments in Ladder Diagram (LD) and Function Block
Diagram (FBD) programs also support rich text.
Comments can be entered for these:
- FBD container
- LD container
- Structured Text container
- Sequential Function Chart container
- Programs, functions, and function blocks
- Defined words
- Array and structure datatypes
- Controller, program, function, and function block variables
- Projects
- Controllers
- Project versioning check-in and labels
- Ethernet ports
- Serial ports
- CIP producers and consumers
- MODBUS slaves and masters
- Libraries
Provide Feedback