I - N

identifier
A unique word used to represent a variable or a constant expression in a program.
Instruction List (IL)
One of the five programming languages defined by the IEC 61131-3 standard for programmable logic controllers. This language was deprecated in the third edition (current) of the standard.
initial situation
Set of the initial steps which represents the context of the program when it is started.
initial step
The logical start of a sequential function chart (SFC).
This is the step that is activated when the program starts.
initial value
Value which has a variable when the virtual machine (application) starts the execution of the controller. The initial value of a variable can be the default value, a value given by the user when the variable is defined or the value of the retained variable after the virtual machine has stopped.
input
The direction of a variable or a device. An input variable is connected to an input channel of an input device.
input parameter
Input argument of a function or a function block. These parameters can only be read by function or function block. A parameter is characterized by a type.
instance of a function block
A copy of the internal data of a function block that persists from one call to the other. This word is used, by extension, to say that a program calls a function block instance and not the function block itself.
instruction
A mnemonic and data address defining an operation to be performed by the controller. A rung in a program consists of a set of input and output instructions. The input instructions are evaluated by the controller as being True or False. In turn, the controller sets the output instructions to True or False.
Each instruction is entered on one line of text.
integer (INT)
An atomic data type consisting of a word used to store a 16-bit signed integer value (-32,768 to +32,767).
Basic type that can be used to define a variable, a parameter, or a device.
internal variable
A variable that is not linked to an input or output device.
internal binding list
The view displaying the resource links and internal variable bindings defined for a project.
I/O binding
A virtual connection between two software elements.
I/O complex device
Element grouping several simple I/O (input and output) devices. This provides the means for manufacturers to mix types and directions. The implementation of the I/O driver of an I/O complex device corresponds to the implementation of the drivers of all contained I/O simple devices. OEM parameters enable providing parameters to I/O complex devices.
I/O device
Element grouping several channels of the same type and direction. These can be either an I/O Simple Device or an I/O Complex Device.
I/O simple device
An I/O simple device corresponds to a piece of equipment having inputs or outputs, such as an I/O board. OEM parameters enable providing parameters to I/O simple devices. Integrators define I/O simple devices.
I/O variable
A variable connected to an input or output device. An I/O variable must be connected on a channel of an I/O device.
An array can be connected to an I/O device if all elements are connected to contiguous channels, the type of the array must be the same type as the I/O device.
I/O wiring
Definition of the links between the variables of the Project and the channels of the I/O devices existing on the Target system.
IXL
ISaGRAF®
eXchange Layer. The protocol for communications between
ISaGRAF
-based components.
jump
A change in the normal sequence of program execution by executing an instruction that alters the program counter (sometimes called a branch). In ladder programs, a JUMP (JMP) instruction causes execution to jump to a labeled rung.
keywords
Terms that have special meanings in a programming language. These terms are reserved and cannot be used as user-defined identifiers for variables, routines, or other elements.
label
The identifier for an instruction within a program. Labels can also be used for jump operations.
ladder diagram
An industry standard for representing relay control logic.
link
A graphic component connecting elements in a diagram.
literal
A value that is expressed as itself rather than as a variable's value or the result of an expression.
local scope
The scope of a declaration applying to only one program.
locked I/O
Input or output variable, disconnected logically from the corresponding I/O device, by a "lock" command.
long integer (LINT)
Signed integer 64-bit format. Basic type that can be used to define a variable, a parameter, or a device.
long real (LREAL)
Type of a variable, stored in a floating IEEE double precision 64-bit format. Basic type that can be used to define a variable, a parameter, or a device.
long word (LWORD)
Unsigned long word 64-bit format. Basic type that can be used to define a variable, a parameter, or a device.
modifier (IL)
Single character put at the end of an IL operation keyword, which modifies the meaning of the operation.
network
The term network is used in different contexts:
  • The means of communication between the target platform and their clients.
  • For the execution order of graphic programs, a sequence of connected blocks.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal