SIN
Yields the Sine of a REAL value.

Arguments | |||
|---|---|---|---|
IN | IN | REAL | Any REAL value |
SIN | Q | REAL | Sine of the input value (in set [-1.0 .. +1.0]) |
Example
(* FBD Program using "SIN" and "ASIN" Functions *)

(* ST Equivalence: *)
sine := SIN (angle); result := ASIN (sine); (* result is equal to angle *)
Provide Feedback