ROR (Rotation Right)
Rotates the DINT type input by NbR bits to the right in a circular form and fills the bits on the left with the bits that are rotated.


Arguments | |||
|---|---|---|---|
IN | IN | DINT | Any integer value |
NbR | NbR | DINT | Number of 1 bit rotations (in set [1..31]) |
ROR | Q | DINT | Right rotated value no effect if NbR <= 0 |
Example
(* FBD Program using "ROR" Function *)

(* ST Equivalence: *)
result := ROR (register, 1); (* register = 2#0100_1101_0011_0101 *) (* result = 2#1010_0110_1001_1010 *)
Provide Feedback