Right Power Rails

Right Power Rails are graphic components of Functional Block Diagram (FBD) programs that represent the right boundary of a rung.
You can link right power rails to left power rails and many FBD and Ladder Diagram (LD) elements, including variables, blocks, vertical bars, coils, and contacts.
To insert a right power rail
  • From the
    Toolbox
    , drag the right power rail element into the language container.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal