Regions
Regions delineate and group together areas of a Function Block Diagram (FBD) program organization unit (POU). A region consists of a header and a delineated zone grouping together elements. The header section enables entering free-format text. After entering text in the header, click elsewhere in the region to exit editing mode. When moving the location of a region in the language container, also move all the content grouped within. Resize regions.
![]() | ![]() |
Task | Procedure |
|---|---|
Insert a region | From the Toolbox , drag the region element into the language container. |
Move a region |
|
Provide Feedback