Comments

Comments are in rich text and inserted anywhere in the Functional Block Diagram (FBD) program organization unit (POU), for documentation purposes only.
After entering text, click elsewhere in the workspace to 'validate' the comment.
Expand and collapse comment elements that display in the workspace by clicking the maximize and minimize buttons. Also resize comments.
Minimize
fbd_c
Maximize
fbd_c1
To insert a comment
  1. From the
    Toolbox
    , drag the comment element into the language container.
  2. In the language container, double-click the comment, then type the required text within the space provided.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal