Coils
Coils are graphic components of Ladder Diagram (LD) programs that can be used in Function
Block Diagram (FBD) programs representing the assignment of Boolean outputs. A coil
represents an action. It must be connected on the left to a Boolean symbol, such as a
contact or the Boolean output of a block.
These types of coils are available from the FBD stencil:
- Direct Coil
- Reverse Coil
- Set Coil
- Reset Coil
Change the type of a coil at any time after insertion.
When inserting coils in program organization units (POUs), assign variables using the
Variable Selector
. Names of assigned variables are displayed above the coil
elements within POUs. Replace existing variables by double-clicking the variable names
to access the Variable Selector
or by single-clicking variable names to select
from drop-down combo boxes containing the global and local variables. Also, single-click
existing variables, then type literal values in the text boxes provided. When inserting
literal values that begin with a letter or an underscore, enclose the variable name in
single quotes as follows: 'abc'.- Select a variable from the drop-down combo-box:

- Type a literal value in the text box:

Task | Procedure |
Insert a coil |
|
Insert a parallel coil |
|
Change the type of a coil |
|
Provide Feedback