Group Field Power Current
Reports the total current drawn from the field power supply by the active digital output modules in a group. Accuracy is
10%.
10%.Direction | Input to the application from the controller |
Type | DINT |
Values | 0 to 8,000 mA or larger (limited by the capacity of the DINT variable) |
Provide Feedback