Controller Status
Access real-time status information for all controllers in a project:
Name | Name of the controller. |
|---|---|
Status | Status of the controller:
Controller statuses also display with a system health condition: Healthy, Faulted, or Warning. |
Locked Variables | Number of locked input and output variables for the controller. |
Cycle Time | Current cycle time of the controller. |
Locked By | Name of the user that applied read-only mode to the controller. |
Password Protected | Indication that the controller is password-protected. True indicates a password-protected controller. |
When viewing the
Controller Status
, the Name
column displays icons that indicate the connection status of the controllers.![]() | Indicates a healthy, running controller having a good system health |
![]() | Indicates a faulted controller having a bad system health |
![]() | Indicates any other condition |
To access controller status information
- From theViewmenu, clickController Status.
Provide Feedback