Resolve invalid CIP links
After opening an AADvance project, if the
Output
window displays invalid CIP produce link or invalid CIP consume link, remove the CIP variable, and then return the deleted CIP variable to the project.To resolve invalid CIP links
- InCommunication View, double-click the CIP produce or CIP consume link.
- Select the CIP producer variable or the CIP consumer variable with the invalid CIP link.
- SelectRemove Selected.
- Return the deleted CIP variable.
- SelectAdd Variable.
- Select the deleted variable.
- SelectOK.
- Save the project.TIP: When you open or build the AADvance project, theOutputwindow no longer displays the invalid CIP links.
Provide Feedback