Configuring a Peer-to-Peer Network
When configuring the Peer-to-Peer network, define these settings:
Network ID | The number identifying the network for the controller. Possible values range from
1 to 8. |
Peer ID | The number identifying the controller IP address in the Peer List. Possible
values range from 1 to 40. |
To configure a peer-to-peer network
- In the Communication View, expand the required controller, then right-clickPeer-to-Peer, and then clickAdd Network.TheNetwork Configurationdialog box displays.
- In theNetwork Configurationdialog box, set the Network ID and Peer ID, and then clickOK.
- (optional) To delete a peer-to-peer subnet, in the Communication View, right-click the network instance to remove, and then clickDelete.The Network with subnets and data blocks are deleted.
Provide Feedback