Application Memory Usage Tools
The Actual Application Memory Usage and Estimated Application Memory Usage tools
determine the impact of application changes before you apply them to AADvance
controllers.
The tools provide the following data:
- Estimated application memory usage for application downloads and updates before they are applied to a controller.
- Actual application memory usage for applications running on controllers.
To access the application memory usage tools, perform the following action:
From the
Application view
, right-click a controller name and
select Actual Application Memory Usage
or
Estimated Application Memory Usage
.Provide Feedback