ODD
Tests the parity of an integer: result is odd or even.

Arguments | |||
|---|---|---|---|
IN | IN | DINT | Any signed integer value |
Odd | Q | DINT | TRUE if input value is odd FALSE if input value is even |
Example
(* FBD Program using "ODD" Function *)

(* ST Equivalence: *)
If Not (ODD (16#1234)) Then Return; End_if; value := 16#1234 + 1; (* makes value always even *)
Provide Feedback