LOG
Calculates the logarithm (base 10) of a real value.

Arguments | |||
|---|---|---|---|
IN | IN | REAL | Must be greater than zero |
LOG | Q | REAL | Logarithm (base 10) of the input value |
Example
(* FBD Program using "LOG" Function *)

(* ST Equivalence: *)
xpos := ABS (xval); xlog := LOG (xpos);
Provide Feedback