COS
Calculates the cosine of a real value.

Arguments | |||
|---|---|---|---|
IN | IN | REAL | Any REAL value |
COS | Q | REAL | Cosine of the input value (in set [-1.0 .. +1.0]) |
Example
(* FBD Program using "COS" and "ACOS" Functions *)

(* ST Equivalence: *)
cosine := COS (angle); result := ACOS (cosine); (* result is equal to angle *)
Provide Feedback