TSTART Statement
Starts the counting of a timer variable. The timer value is not modified by the TSTART command,for example, the counting starts from the current value of the timer.
TSTART Statement | |
|---|---|
Name | TSTART |
Syntax | TSTART ( <timer_variable> ); |
Operands | Any inactive timer variable |
Return value | (none) |
Example
(* ST program using the TSTART statement *) bo100 := TRUE; (* boolean output *) tm_ctrl := t#0s; TSTART(tm_ctrl);
To insert a TSTART statement
- In the language container, typeTSTART.
Provide Feedback