Use FactoryTalk Security with AADvance-Trusted SIS Workstation software
FactoryTalk Security
with AADvance-Trusted SIS Workstation software
The
FactoryTalk Security
software allows you to control actions on your projects based on:- the user who is signed in.
- the project the user is attempting to modify.
- the computer from which the user is attempting to modify the project.
TIP:
The security feature is intended to prevent accidental unauthorized action to
your project and to
Trusted
controller equipment. It is important to note
that while the feature does provide some protection against intentional unauthorized action,
it does not provide protection against action conducted by system hackers. You should put in
place additional preventative measures against unwanted actions.FactoryTalk Security
grants or denies action based on:- User ID
- Computer name
- Action name (that is, the activity the user is trying to perform, such as configure I/O devices, or download an application)
IMPORTANT:
Before you use this feature, read the
FactoryTalk Security System
Configuration Guide
, which is available in the Rockwell Automation Literature Library:
rockwellautomation.com/en-us/support/documentation/literature-library.html
TIP:
AADvance-Trusted SIS Workstation software
startup might open slowly when FactoryTalk
Services version 6.31.00 or later is installed.Users who do not
plan to use the permission-based control feature are therefore advised not to install
it.
If
FactoryTalk
Services version 6.31.00 or later must be
installed, users are advised to deactivate the Use single sign-on
security policy
in the FactoryTalk Administration Console
.Security policy considerations
When you use
FactoryTalk Administration Console
to configure securable actions, security settings are obtained from the FactoryTalk
Network Directory.Provide Feedback