Add a program from an exchange file
Import programs previously exported as exchange files (*.txf). Importing exchange files enables reusing programs in different
Trusted®
projects.
TIP:
Importing a program, function, or function block
imports its logic, local variables, local defined words, and description. Program, function,
and function block comments, Diary files, and Modbus® extended attributes are not
imported.
When importing a program organization unit (POU), specify a unique name within the project.
To add a program from an exchange file
- In theApplication View, right-clickPrograms, point toAdd Programs, and then clickExisting Program....TIP: Alternatively, add an existing program fromFile > Add > Existing Program...
- In theSelect Exchange Filedialog box, locate theTrustedexchange file containing the program, and then clickOpen. The program is imported into the project.
Provide Feedback