Division
Divides two integer or real variables (the first divided by the second).

Arguments | ||
|---|---|---|
IN1 | DINT - REAL | can be integer or real format (operand) |
IN2 | DINT - REAL | non-zero integer or real value (divisor) (IN1 and IN2 must have the same format) |
Q | DINT - REAL | integer or real division of IN1 by IN2 |
Example
(* FBD example with Division Operators *)

(* ST Equivalence: *)
ao10 := ai101 / ai102;
ao5 := (ai51 / 1) / ai53;
Provide Feedback