Reserved Keywords
Reserved keywords are unavailable for use as names of POUs or variables.
Keywords | |
|---|---|
A | ABS, ACOS, ADD, ANA, AND, AND_MASK, ANDN, ARRAY, ASIN, AT, ATAN, |
B | BCD_TO_BOOL, BCD_TO_INT, BCD_TO_REAL, BCD_TO_STRING, BCD_TO_TIME, BINDING, BOO, BOOL, BOOL_TO_BCD, BOOL_TO_INT, BOOL_TO_REAL, BOOL_TO_STRING, BOOL_TO_TIME, BY, BYTE, |
C | CAL, CALC, CALCN, CALN, CALNC, CASE, CONCAT, CONSTANT, COS, |
D | DATE, DATE_AND_TIME, DELETE, DINT, DIV, DO, DT, DWORD, |
E | ELSE, ELSIF, EN, END_CASE, END_FOR, END_FUNCTION, END_IF, END_PROGRAM, END_REPEAT, END_RESOURCE, END_STRUCT, END_TYPE, END_VAR, END_WHILE, ENO, EQ, EXIT, EXP, EXPT, |
F | FALSE, FIND, FOR, FUNCTION, |
G | GE, GFREEZE, GKILL, GLOBALVARIABLE, GRST, GSTART, GSTATUS, GT, |
H | HEADER, |
I | IF, INSERT, INT, INT_TO_BCD, INT_TO_BOOL, INT_TO_REAL, INT_TO_STRING, INT_TO_TIME, IO, |
J | JMP, JMPC, JMPCN, JMPN, JMPNC, |
L | LD, LDN, LE, LEFT, LEN, LIMIT, LINT, LN, LOG, LREAL, LT, LWORD, |
M | MAX, MID, MIN, MOD, MOVE, MSG, MUL, MUX, |
N | NE, NOT, |
O | OF, ON, OPERATE, OR, OR_MASK, ORN, |
P | PROGRAM |
R | R, READ_ONLY, READ_WRITE, REAL, REAL_TO_BCD, REAL_TO_BOOL, REAL_TO_INT, REAL_TO_STRING, REAL_TO_TIME, REPEAT, REPLACE, RESOURCE, RET, RETAIN, RETC, RETCN, RETN, RETNC, RETURN, RIGHT, ROL, ROR, |
S | S, SEL, SET, SHL, SHR, SIN, SINT, SQRT, ST, STN, STRING, STRING_TO_BCD, STRING_TO_BOOL, STRING_TO_INT, STRING_TO_REAL, STRING_TO_TIME, STRUCT, SUB, SUB_DATE_DATE, SYS_ERR_READ, SYS_ERR_TEST, SYS_INITALL, SYS_INITANA, SYS_INITBOO, SYS_INITTMR, SYS_RESTALL, SYS_RESTANA, SYS_RESTBOO, SYS_RESTTMR, SYS_SAVALL, SYS_SAVANA, SYS_SAVBOO, SYS_SAVTMR, SYS_TALLOWED, SYS_TCURRENT, SYS_TMAXIMUM, SYS_TOVERFLOW, SYS_TRESET, SYS_TWRITE, SYSTEM, |
T | TAN, TASK, THEN, TIME, TIME_OF_DAY, TIME_TO_BCD, TIME_TO_BOOL, TIME_TO_INT, TIME_TO_REAL, TIME_TO_STRING, TMR, TO, TOD, TRUE, TSTART, TSTOP, TYPE, |
U | UDINT, UINT, ULINT, UNTIL, USINT, |
V | VAR, VAR_ACCESS, VAR_EXTERNAL, VAR_GLOBAL, VAR_IN_OUT, VAR_INPUT, VAR_OUTPUT |
W | WHILE, WITH, WORD |
X | XOR, XOR_MASK, XORN |
Provide Feedback