Align Objects

Align objects relative to their left side, right side, top edge, or bottom edge. Elements align relative to the first element selected.
Once objects are selected, choose to align them with commands from the
Layout
menu available from the contextual menu or use the arrow keys.
To align and position objects
  1. Select the objects to align starting with the element to use as reference for the alignment.
  2. Right-click the elements, point to
    Layout
    , then click the required alignment command:
    • Align Left
    • Align Center
    • Align Right
    • Align Top
    • Align Middle
    • Align Bottom
The objects are aligned in the selected direction in reference to the first selected item.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal