Unwire channels of an I/O device
Unwire the channels of an I/O device to use the directly represented variable rather than a wired variable. Unwire all channels or individual channels of an I/O device.
To unwire channels of an I/O device
- Access the I/O Wiring for the device.
- Do one of these:
- To unwire all wired channels for the I/O device, from theI/O Wiringtoolbar, click
. - To unwire individual channels of the I/O device, right-click the channel, and then selectUnwire selected channels.TIP: To unwire multiple channels, hold theCtrlbutton while selecting each required channel.
Provide Feedback