Lock and unlock an I/O variable
When debugging, choose to lock, unlock, and force the values of I/O variables.
To lock and unlock an I/O variable
- Access the I/O Wiring for the device and select the channel to lock or unlock.TIP: To lock or unlock multiple channels, holdCtrlwhile selecting each required channel.
- To lock or unlock the variable, right-click the variable, and then select or clearToggle lock on selected channels.
Provide Feedback