I/O wiring keyboard shortcuts
The following keyboard shortcuts are available for use with I/O wiring. Some shortcuts do not apply or may differ while debugging.
Keyboard Shortcut | Description |
|---|---|
Ctrl+N | Adds a device (not available while debugging). |
Ctrl+F | Unwires all channels of selected devices (not available while debugging). |
Ctrl+R | Unwires selected channels of a device (not available while debugging). |
Ctrl+H | Toggles between a real or virtual I/O device (not available while debugging). |
Ctrl+L | While debugging, toggles between locking and unlocking selected channels. |
Provide Feedback