Display I/O device information
Display I/O device information for simple and complex devices. For simple devices, change the order on the rack list. For simple devices, read-only information includes the order on the rack list, the number of channels, the data type for wiring, and a description.
TIP:
For simple devices, the DINT data type also allows
wiring real variables.
To display I/O device information
- From the rack list, expand the required I/O device by clicking
. - ClickInfo to view information about the device.
Provide Feedback