Error Statistics (ERRSTAT)
Several process control functions and function blocks may generate error conditions causing these ERRSTAT counters to increment: reversed parameters, incorrect parameter values, overflow conditions, underflow conditions, and divide by zero.

Parameter values for the ERRSTAT function block:
Parameter | Data Type | Description | ||
|---|---|---|---|---|
RESET | BOOL | When TRUE, resets the error counters to
zero. | ||
Reversed | DINT | Reversed parameters error counter. The count increments on each execution of the
function when the parameters are reversed. The initial value is zero. | ||
Param | DINT | Incorrect parameter values error counter. The count increments on each execution
of the function when the parameter value is incorrect. The initial value is zero. | ||
Overflow | DINT | Overflow condition error counter. The count increments on each execution of the
function when the overflow condition occurs. The initial value is zero. | ||
Underflow | DINT | Underflow condition error counter. The count increments on each execution of the
function when the underflow condition occurs. The initial value is zero. | ||
ZeroDivide | DINT | Divide by zero error counter. The count increments on each execution of the
function when the divide by zero error occurs. The initial value is zero. | ||
TIP:
Counter values do not wrap to zero. Counter overflow
conditions return a value of -1.
Function Block Diagram Example

Structured Text Example
ERRSTAT(Reset_count); Reversed_count := ERRSTAT.Reversed; IncorrectParam_count := ERRSTAT.Param; Overflow_count := ERRSTAT.Overflow; Underflow_count := ERRSTAT.Underflow; ZeroDivide_COUNT := ERRSTAT.ZeroDivide;
Provide Feedback