Export a function
Export functions as exchange files (*.txf) to import them into different projects.
Importing exchange files enables reusing functions in different
Trusted®
projects. Export individual functions.
TIP:
Exporting a program, function, or function block
exports its logic, local variables, local defined words, and description. Program, function,
and function block comments, Diary files, and Modbus® extended attributes are not
exported.
To export a function
- In theApplication View, right-click the function, and then clickExport....
- In theSave Function Asdialog box, browse for the location to store theTrustedexchange file, and then clickSave. The function is exported as an exchange file.
Provide Feedback