CTUD
Counts (integers) from 0 up to a given value in increments of 1 or from a given value down
to 0 in increments of 1.
IMPORTANT:
The CTUD block does not detect the rising edges
and falling edges of the counting inputs (CU and CD). The block must be associated with an
R_TRIG or F_TRIG block to create a pulse counter.

Arguments | ||
|---|---|---|
CU | BOOL | Up-counting (when CU is TRUE) |
CD | BOOL | Down-counting (when CD is TRUE) |
RESET | BOOL | Reset command (dominant) (CV = 0 when RESET is TRUE) |
LOAD | BOOL | Load command (CV = PV when LOAD is TRUE) |
PV | DINT | Programmed maximum value |
QU | BOOL | Overflow: TRUE when CV >= PV |
QD | BOOL | Underflow: TRUE when CV <= 0 |
CV | DINT | Counter result |
Example
(* FBD program using the CTUD block *)

(* ST Equivalence: We suppose R_TRIG1 and R_TRIG2 are two instances of R_TRIG block and
CTUD1 is an instance of CTUD block*)
R_TRIG1(add_elt); R_TRIG2(sub_elt); CTUD1(R_TRIG1.Q, R_TRIG2.Q, reset_cmd, load_cmd,100); full := CTUD1.QU; empty := CTUD1.QD; nb_elt := CTUD1.CV;
Provide Feedback