Vertical Bars

Vertical bars are graphic components of Function Block Diagram (FBD) programs enables closing multiple parallel links. More than one horizontal links on the left side of a vertical bar are connected to one link on the right side. The Boolean state of the right end is the logical OR between all the left extremities.
fbd_vb1_cam3
To insert a vertical bar
  • From the
    Toolbox
    , drag the vertical bar element into the language container.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal