Create a defined word
Create defined words to use in projects. Defined words are identifier names that replace literal expressions, boolean expressions, reserved keywords, or complex ST expressions.
To create a defined word
- From theApplication View, double-clickDefined Words.
- In theDefined Wordsgrid, define the required properties:
- Name-- Name of the defined word. Limited to 32 characters beginning with a letter or single underscore followed by letters, digits, and single underscore characters. Names cannot be reserved words, defined words, or data types. Names must be unique.
- Equivalent-- String replacing the defined word during compilation. For example, the defined word "PI" is replaced by its equivalent "3.14159". Limited to 255 characters.TIP: Do not use spaces for the equivalent string. Using a space prevents saving of the new defined word.
- Comment-- Plain text.
- PressEnter.
Provide Feedback