View cross references of a defined word
Update the
Cross Reference Browser
to display current cross references in the project.The properties of defined word cross references appear in the
Elements
pane of the Cross Reference Browser
:Property | Description |
|---|---|
Name | Name of the defined word. |
Count | Total number of cross references existing for a defined word in the project. |
Equivalent | String replacing the defined word during compilation. |
Scope | Project using the defined word. |
Comment | Free-format text |
To view cross references of a defined word
- In theCross Reference Browser, select theDefined Wordsview, and then click
Update Cross Reference Data. The cross references update. - In theElementspane, select the defined word. Cross references for the selected defined word appear in theReferencespane.
- Right-click the cross reference and clickGo to Reference. The language container displays the cross reference of the defined word.
Provide Feedback