Specify Documentation Generator options
Specify the default Sections Template and the
Word®
options for the generated documentation. The selected Sections Template modifies the items listed in the Sections pane of the Documentation Generator. The Word
options modifies the different aspects of the print output including page orientation, paper format, margins, Word template, scaling of diagrams, link type, and comment style.To specify the Documentation Generator options
- From theToolsmenu, clickOptions...
- In theOptionsdialog box, do these:
- ExpandDocumentGenerator, clickGeneral, then select the required default Sections Template.
- ClickWordand specify the required settings.
- ClickOK.
Provide Feedback