ISaVIEW Animation Settings

Use the animation settings to customize the animation settings for ISaVIEW screens including action, displacement, rotation, and size. Also define the refresh rate of ISaVIEW screens and their default background color.
To customize the animation settings for ISaVIEW screens
  1. From the
    Tools
    menu, click
    Options
    .
  2. From the
    Options
    dialog box, expand
    ISaVIEW
    Settings
    , and then click
    ISaVIEW
    Animation
    Settings
    .
  3. Customize the required settings, and then click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal