Setting Environment Options

Define the environment options for the following:
  • Find and Replace Settings
  • Help Page Source
  • Import and Export Settings
  • Shortcut Keyboard Combinations
  • Startup
  • Tabs and Windows
Modify the general settings for the
AADvance-Trusted SIS Workstation software®
by accessing the general environment options. Some changes to the general settings take effect after restarting the software.
  • Visual experience
    , indicates the color theme to use in the development environment and specifies whether the visual experience is set automatically or explicitly. For the color theme, the possible colors are blue and light. For the visual experience, the adjustment may change the display of colors from gradients to flat colors, or it may restrict the use of animations in menus or popup windows. Enabling the full visual experience includes gradients and animations. Clear this option when using remote desktop connections or older graphics adapters because these features may have poor performance in such cases. Use hardware graphics acceleration if available rather than software acceleration.
  • Window menu
    , indicates the number of windows (ranging from 1 to 24) that display in the Windows list of the
    Window
    menu. For the number of items shown in the
    Window
    menu, the default value is 10.
  • Recently used
    , indicates the number of recently used files displayed in menus. The items shown in recently used lists field defines the number of recent projects and files (ranging from 1 to 24) that display in the
    File
    menu. For the number of items shown in recently used lists, the default value is 4.
  • Show status bar
    , displays the status bar showing progress information for ongoing operations.
  • Close button affects active tool window only
    , enables the Close button to shut down the active window only. This option is selected by default.
  • Auto Hide button affects active tool window only
    , enables
    Auto Hide
    to hide the active window only.
To access the general environment options
  1. From the
    Tools
    menu, click
    Options
    .
  2. In the
    Options
    dialog box, expand
    Environment
    , then click
    General
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal