Define I/O Wiring Settings

Specify settings for
Trusted®
I/O wiring.
  • Always keep devices expanded
    , specifies whether devices are expanded to display information such as the slot order, number of channels, data type, and description
  • Show empty device slots
    , specifies whether empty device slots are displayed when viewing I/O wiring
  • Show full device names
    , specifies whether I/O devices are displayed with their full names beside the slot number
  • Prompt on device removal
    , specifies whether to prompt users before removing devices
To specify the
Trusted
I/O wiring settings
  1. From the
    Tools
    menu, click
    Options
    .
  2. In the
    Options
    dialog box, expand
    I/O Wiring
    , and then click
    General
    .
  3. Specify the settings as required, and then click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal