Generating Documentation
While in design mode, generate documentation for projects, controllers or devices, POUs, variables, and library elements. The output format of the documentation is
Microsoft®
Word®
2010 (*.docx). Use Generate Documentation
to view the project information for a specific time, and search and edit the generated documentation.Install
Microsoft
Word
2010 (or more recent) or another *.docx application to properly view, search, and edit the generated documentation.
TIP:
Microsoft
Word
2013 has a file size limitation that affects generated
documents. Documents generated from projects with large POUs or many variables are unusable
or incomplete. For more information on the Microsoft
Word
2013 file size limitation, see Operating parameter limitations and specifications in
Word. The
Generate Documentation
dialog box is separated into three panes: Document Options
, Sections
, and TOC Preview
. Selections in a pane affect what displays in the next pane (from left to right). Changes in the Document Options
pane affect what displays in the Sections
pane and changes in the Sections
pane affect the TOC Preview
pane.
Options for the
Document Options
pane are:Option | Description | Possible Values |
|---|---|---|
Sections Template | Template in XML format defining the Sections to be generated in the documentation and their hierarchy. The selected Sections Template affects the items that display in the Sections and TOC Preview panes. The templates are located in the following directory: %PUBLIC%\Public Documents\SIS Workstation < version >\Templates\DocumentGenerator | DefaultTemplate, NoISaview Template, or a user-defined *.xml template. The default value is DefaultTemplate. |
Orientation | Orientation of the page | Portrait or Landscape. The default value is Landscape. |
Page size | Size of the page | Letter, Legal, Statement, Executive, A3, A4, A5, B4 (JIS), B5 (JIS), 11x17, Envelope #10, Envelope DL, Envelope C5, Envelope B5, Envelope Monarch, Japanese Postcard, A6, Double Japan Postcard Rotated, Executive (JIS), Oficio 8.5x13, 12x18, 8k 273x394 mm, 16k 197x273 mm, or Custom. The default value is Legal. |
Margins | Left, right, top, and bottom margins for the page | Narrow, Normal, Moderate, or Custom. The custom margins range from 0 inches to the maximum size of the page. The default value is Normal. |
Microsoft Word Template | Microsoft Word template in *.dotx format used to define the layout for the title page, table of contents, and tables.The templates are located in the following directory: %PUBLIC%\Public Documents\SIS Workstation < version >\Templates\DocumentGenerator | IsagrafFooter.dotx, Isagraf_NoHeader.dotx, or a user-defined *.dotx template. The default template is IsagrafFooter.dotx. |
Diagram Scaling | Scaling for all diagrams that display in the generated documentation. | 25%, 50%, 75%, 100%, 125%, 150%, 175%, 200%, 300%, 400%, 500%, Fit to Page, or Custom. When selecting the Custom scaling, a spin box appears enabling the user to select the scaling value. The default value is 100%. |
Link Type | Type of links in the documentation. | None, Only Bookmarked, Cross Reference, or Hyperlink. The default value is None. |
Comment Style | How comments display in the documentation. This option does not affect how comments are displayed in graphical POU diagrams. | // comment, /* comment */, or (* comment *). The default value is (* comment *). |
Selecting a Sections Template in the
button displays the
Document Options
pane modifies the items listed in the Sections
pane. The Title Page and Table of contents items are always available for selection in the Sections
pane. The
button displays the Variable Settings
dialog box and is used to specify how to sort the variables in the generated documentation.- For AADvance projects, sort variables by Name, Comment, Alias, Data Type, Wiring, Attribute, Dimension, Initial Value, Direction, or String Size in ascending or descending order.
- ForTrusted®projects, sort variables by Name, Comment, Data Type, Wiring, Initial Value, Attribute, Direction, String Size, Modbus Address, Message True, Message False, Retained, or Unit in ascending or descending order.
The items selected in the
Sections
pane modify the items that display in the tree view of the TOC Preview
pane. Select or clear items in the TOC Preview
pane. The final selection in the TOC Preview
pane displays what is generated in the documentation.The items that display in the
Sections
and TOC Preview
panes also depend on the element selected in the Application View
when using the Generate Documentation
command.- Example: if a POU is selected in aTrustedapplication, only associated sections (diary, local variables, and the POU diagram) display in theGenerate Documentationdialog box.
When the project is selected in the
Application View
, all sections (project, global variables, defined words, structures, arrays, targets, etc.) display in the dialog box. Where a project, resource, device, POU, or library element is not selected, the documentation generator tries to find the associated element.- Example: if Local Variables of a POU are selected, the POU is considered the associated element and therefore displays in theSectionsandTOC Previewpanes. If the document generator is unable to find an associated element, theGenerate Documentationcommand does not appear in theFilemenu.
The document generator retains the selections made in the three panes for each element across project sessions. Reset the pane selections by clicking
Default Settings
.Users can create their own custom templates for the Sections Templates (*.xml) and
Microsoft
Word
templates (*.dotx). When creating a custom XML template, the following syntax must be used:Section | Description |
|---|---|
TitlePageSection | The title page |
TOCPageSection | The table of contents |
SolutionSection | The title of the solution name |
ProjectSection | The title of the project name |
ArraysSection | The table displaying arrays |
StructuresSection | The table displaying structures |
DefinedWordsSection | The table displaying defined words |
ConfigurationSection | The title of the controller or device name and the table displaying network links |
ProgramSection | The title of the program name |
POUContentSection | The POU diagrams |
VariableSection | The tables for local and global variables. Also displays the extended attributes for global variables. |
IOWiringSection | The I\O wiring table |
TargetSection | The table displaying the targets |
BindingSection | The table displaying the bindings |
When creating a custom
Microsoft
Word
template (*.dotx), how sections display may be modified, but the following styles and table styles defined by Microsoft
Word
or AADvance-Trusted SIS Workstation software®
must be maintained:Style | Description |
|---|---|
Heading 1 | How Header 1 displays in the documentation. |
Heading 2 | How Header 2 displays in the documentation. |
Heading 3 | How Header 3 displays in the documentation. |
Heading 4 | How Header 4 displays in the documentation. |
Heading 5 | How Header 5 displays in the documentation. |
Heading 6 | How Header 6 displays in the documentation. |
Heading 7 | How Header 7 displays in the documentation. |
Heading 8 | How Header 8 displays in the documentation. |
Heading 9 | How Header 9 displays in the documentation. |
Alias | How the Alias section displays in the documentation. |
Comment | How comments displays in the documentation. |
Table Style | Description |
|---|---|
IOWiring | The tables displaying information for I/O wiring and targets. |
NormalStyle | The tables displaying information for bindings. |
VariableTableStyle | The tables displaying information for variables, arrays, structures, and defined words. |
To generate documentation
- In theApplication View, select the element (project, controller or device, POU, library element, etc.) for which to generate documentation.
- From theFilemenu, clickGenerate Documentation.
- Specify the required options, and then clickGenerate.
- In theSave Asdialog box, specify the file name and save location, and then clickSave.A progress bar appears over theGenerate Documentationdialog box displaying the generation progress. ClickCancelto stop the document generation process. Any files created during the generation process are deleted.Once generation is complete, the *.docx application displays the documentation.
Provide Feedback