External Tools
Launch external tools and applications by adding items to the
Tools
menu. Also create keyboard shortcuts for external tools added to the Tools
menu. Supported file types include .exe, .bat, .com, .cmd, and .pif. When specifying a tool for handling arguments, the required argument is immediately transferred to the tool when the external tool is launched. At this time, choose to edit required arguments. Upon subsequent startups of the external tool from the
Tools
menu, selected arguments are automatically passed to the tool. When Prompt
for
Arguments
is selected, the Arguments
dialog box displays.Define a working directory for tools or commands. Also specify additional arguments when the command is launched.
From the
External
Tools
dialog box, perform these tasks:Task | Procedure |
|---|---|
Add an external tool |
|
Specify a tool for handling arguments | When the specified tool is launched, the required argument is immediately transferred to the tool. Select Prompt for Arguments to edit the argument at launch time.
|
Define a working directory |
|
Provide Feedback
.
.
.