Install Redundancy Firmware
To install redundancy firmware, follow these steps.
- Run the downloaded EXE file.
The executed file installs a DMK firmware file in the download location that is specified in yourControlFLASH Plus®settings.
- Verify that the DMK file is in theControlFLASH Plus®firmware kits location.You can manually move the DMK file if needed.
Provide Feedback