Safety Partner Status Messages

The safety partner display can show these scrolling messages.
Safety Partner Status Messages
Message
Interpretation
L9SP
Standard display text. If there is a major nonrecoverable fault, then the fault code scrolls across the display.
Flash in Progress
A firmware update is in progress. Allow the firmware update to complete without interruption.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal