Obtain Controller Firmware

You can obtain controller firmware in these ways:
  • Install the
    Studio 5000 Logix Designer®
    application and use the packaged firmware.
IMPORTANT:
The firmware that is packaged with the software installation is the initial release of the controller firmware. Subsequent firmware revisions to address anomalies can be released during the life of a product.
We recommend that you check the Product Compatibility and Download Center (PCDC) to determine if later revisions of the controller firmware are available
  • From the PCDC, download revisions of controller firmware, and download controller firmware, associated files, and product release notes.
    ControlFLASH Plus®
    software version 2.00.00 or later provides integration with PCDC for an enhanced experience while you browse for firmware revisions, downloads, release notes, and access to important notices.
Visit the Product Compatibility and Download Center (PCDC) at rok.auto/pcdc.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal