Device Information View

Use Device Information to view device and status information when the device is online.
Use Device Information to:
  • Determine the identity of the device.
  • View the device's current operational state.
  • View whether an owner controller is currently connected to the device.
  • Retrieve the latest information from the device.
  • Reset a device to its power-up state.
Device Information View Example

Device Diagnostics

To view the device diagnostics, select Diagnostics in the Device Information view.
Device Diagnostics Example
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal