No Load Detection
IMPORTANT:
This feature is available only in Current (mA)
mode.
No Load Detection detects when a wire is disconnected from the channel or a missing load
for each output channel. The output range that is used with the analog output module
determines the current below which a load is considered missing.
The
I.Chxx.NoLoad
tag indicates the presence of a no load condition when it is set
to 1.The No Load Detection feature is disabled by default. You must enable the feature in your
Studio 5000 Logix Designer application project. To enable No Load Detection, go to
Channels, then Chxx view and select the Enable No Load Detection checkbox. Select Apply
or OK to save the configuration.
Provide Feedback