PNPOS device options
Use the
Advanced > Device Options
tab on the PNPOS Properties
dialog box to configure device options for the selected Process n-Position Device (PNPOS) instruction.To configure device options for PNPOS instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
. - In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Select theAdvanced > Device Optionstab.
- Enter the number of device positions for the device being controlled or monitored in theNumber of device positionsbox.
- Set theDevice type:
- For a rotary device, selectCircular.
- For a linear device, for which positions 1 and n are at the ends of travel, selectLinear.
- Select theDevice behavior:
- For a circular (rotary) device, select whether the device can move in either direction (clockwise or counterclockwise) or can only rotate clockwise.
- For a linear device, select whether the device can move directly to a new position or must return to position 1 on every move.
- Select check boxes to enable settings based on the device:
- Device has feedback for all positions. Select if the device provides position feedback. This is an engineering configuration.
- Use position feedback setting during move. Clear this check box to bypass the position feedback checking. This is a maintenance bypass function.
- Allow a new position setting during move. Select to accept a new position setting that is received during a move. When this check box is cleared, the device must wait for the previous move to complete.
- Keep output position ON until next move. Latches the position command output until a new position is set.
- Device has indexing cylinders (extend, right, retract, left) with position feedback. Select if the device provides indexing cylinder feedback. This is an engineering configuration.
- Use indexing cylinder position feedback. Clear this check box to bypass the indexing cylinder feedback checking. This is a maintenance bypass function.
- Must unlock/unseal to move, lock/seal when done. Select if the device has a lock or seal and must unlock or unseal before moving.
- Device has locked/unlocked feedback. Select if the device provides lock feedback. This is an engineering configuration.
- Use lock feedback for failure checking. Clear this check box to bypass the lock feedback checking. This is a maintenance bypass function.
- SelectApply.
Provide Feedback