Help menu
The Help menu contains the following commands:
Contents command
Access the Logix Designer Online Help contents.
Instruction Help command
Choose this command to view the instruction set help.
Release Notes command
Choose this command to display the Logix Designer application release notes.
Online Books command
Choose this command to access the
Logix Designer
application online books.Vendor Sample Projects command
Choose this command to launch the
Vendor Sample Projects .pdf
file to access sample projects from Rockwell Automation and several other vendors. Use these sample projects with products from those companies. Refer to the PDF file for more information.
IMPORTANT:
Some browsers (particularly the Edge browser)
will not launch the
Logix Designer
application from the ACD
hyperlinks in the PDF file when configured to open PDF files.About
Logix Designer
command
Display version history, license information, contact information, and additional product information including installed components, installed controller support, installed firmware support, and motion database information.
Provide Feedback