Discard Operand Changes
These actions discard the new value:
- scroll the Routine up or down. This includes using the keyboard, mouse or mouse wheel or auto-scrolling.
- selectEsc
- Edit control or Routine View loses focus
- drop a new Ladder Element on the Routine
- perform some Menu item command
- maximize or iconize the Routine Window
- invoke Help usingF1
- split the Routine Window
Provide Feedback