Reference data outside the Equipment Sequence

A sequence program can require external equipment data such as the level of a tank or the temperature of an oven. Program parameters are used to make that data available within the sequence program by creating a connection to the appropriate tag. This keeps the data required to run the sequence encapsulated within the program.
A sequence program can also have a dependency on another program. For example, create a connection between a sequencing output parameter from one
Equipment Sequence
program to be used as an input parameter by another
Equipment Sequence
program.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal