Port Diagnostics dialog box
Use this dialog box to view the diagnostic information for the port. When the controller is online, you can do the following on the
Port Diagnostics
dialog box.- View the interface and media counters for the port.
- Reset the interface and media counters to zero.
The
Port Diagnostics
dialog box is only available for controllers with an embedded Ethernet port, and the data is only displayed when the controller is online.
TIP:
To open the Port Diagnostics dialog:
- In theController Organizer, expand theI/O Configurationfolder, and double-click the controller.
- On theController Propertiesdialog box, click thePort Configurationtab.
- Click theBrowse(...) button to open thePort Diagnosticsdialog box.
Provide Feedback